earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Enterprise Central, Enterprise Server, FDP Server
Functionalities: Basic Functionality
12/2/2024

Uploading and Downloading a Backup using WebStation

You can upload and download a backup using WebStation.

Show More
action_close

A subset of backup and restore features are available in WebStation.

You can create backups of the server using WebStation. The backup can be downloaded and uploaded from the server.

Scheduled backup must be done using WorkStation.

For more information, see Backup .

To upload and download a backup using WebStation
  1. Click WebStation, click Workspace menu .

  2. Click System .

  3. Click Backup and restore .

  4. In the Backup and restore dialog:

    • Click Upload to upload a backup.

    • Select a backup and click Download to download the selected backup.

  • Backup and Restore Overview
  • Backup and Restore using WebStation
  • Backing up and Restoring using WebStation
  • Backup