earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Device Administrator, FDP Server, ​License Administrator
Functionalities: Engineering
3/6/2025

Confirming the Return of Licenses on the License Activation Server (FNO)

You confirm the return of licenses so that License Activation Server can active the returned licenses again.

This step must be done a computer that is connected to Internet and has access to License Activation Server.

Show More
action_close

Device Administrator is used to manage licenses on field servers.

Software and Features that Require Licenses

A number of software features need licenses.

For more information, see Software and Features that Require Licenses .

Entitlements, Products, and Licenses

Licenses are bought as products and delivered in Entitlements. An Entitlement is a container that can contain several products. The products contain the licenses and they can differ in quantity and contents.

Field Server Licensing Workflow

Use one of these workflows, depending on if the field servers are connected or not connected to the Internet.

For more information, see Field Server Licensing on Field Servers Connected to Internet Workflow .

For more information, see Field Server Licensing on Field Servers not Connected to Internet Workflow .

Certificates

It is recommended to use HTTPS for the communication between Device Administrator and field servers when you manage licenses.

For more information, see Certificates Managed using Device Administrator .

Return Licenses on Field Servers

You can return licenses from field servers.

For more information, see Return Licenses on Field Servers .

To confirm the return of licenses on the License Activation Server (FNO)
  1. In Device Administrator, click Servers .

  2. Select Show Licenses .

  3. Select the automation servers.

  4. Click Return .

  5. Click Confirm return of licenses on the License Activation Server (FNO) .

  6. Click OK .

  7. In the Confirmation field, browse to the confirmation file.

  8. Click Upload .

  9. Click Close .

  • Field Server Licensing Overview
  • Creating the Request Files
  • Uploading Request Files to License Activation Server (FNO)
  • Sending the Response Files to the Field Server when Activating or Reclaiming Licenses
  • Confirming the Return of Licenses on the License Activation Server (FNO)