earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Enterprise Central, Enterprise Server, FDP Server
Functionalities: Alarms
10/30/2025

XLSX Template Tab

Use the XLSX Template tab to configure a template.

 
action_zoom_plus_stroke XLSX Template tab
Figure: XLSX Template tab

Table: XLSX Template tab

Component

Description

Edit with spreadsheet editor

Click to open the XLSX spreadsheet for editing.

Import XLSX file

Click to import an XLSX file.

Go to report

Click to navigate to the XLSX report.

Generate preview

Preview generated report

Click to preview a generated report including all data.

Preview generated report without data

Click to preview the substitution codes without any data. Use this preview to make sure that the context does not overlap.

Copy to spreadsheet

Displays the substitution code to be used in the spreadsheet. Copy the substitution code and paste it into the spreadsheet where you want to display it.

 
action_zoom_plus_stroke

Add context

Click to add a context to the template. For more information, see Context Configuration .

 
action_zoom_plus_stroke

Edit context

Click to open the Context Configuration dialog and edit the template. For more information, see Context Configuration .

 
action_zoom_plus_stroke

Remove context

Click to remove a context from the template.

Binding data

Click to open the Binding data tab, to add, edit or remove binding data.

  • XLSX Reports Overview
  • XLSX Reports Workflow
  • XLSX Report Template Tab
  • XLSX Template Tab
  • Context Configuration – Template Tab
  • Context Configuration – Calculation Tab
  • Context Configuration – Misc Tab