earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Enterprise Central, Enterprise Server, FDP Server
Functionalities: Alarms
12/3/2024

Editing a Checklist

You edit a checklist to change the description of a step, or to rearrange the step order.

To edit a checklist
  1. In WorkStation, in the System Tree pane, select the EcoStruxure BMS server you want to configure.

  2. Click the Control Panel tab.

  3. Click Checklists .

  4. In the Checklist view, click the Edit checklist button

     
    action_zoom_plus_stroke
    .

    Note:
    • To permanently remove a checklist, click the Remove checklist button

       
      action_zoom_plus_stroke
      .

  5. In the Edit Checklist dialog box, in the Name box, type the name of the new checklist.

  6. In the Description box, type a description for the checklist.

  7. Select a step in the checklist and click the Edit step button

     
    action_zoom_plus_stroke
    to edit the checklist step.

    Note:
    • In the Edit checklist step dialog box you can add new steps to the checklist by clicking the Add step

       
      action_zoom_plus_stroke
      button, or remove existing steps by clicking the Remove step
       
      action_zoom_plus_stroke
      button .

  8. In the Edit checklist step dialog box, in the Name box, type the new text for the step.

  9. Click OK .

  10. Select a step in the checklist and click the Move step up button

     
    action_zoom_plus_stroke
    to move the step upwards in the checklist.

  11. Select a step in the checklist and click the Move step down button

     
    action_zoom_plus_stroke
    to move the step downwards in the checklist.

  12. In the Edit Checklist dialog box, click OK .

  13. Click the Save button

     
    action_zoom_plus_stroke
    .

  • Alarm Functions
  • Alarms Overview
  • User Actions
  • Alarm Control Panel – Checklists View
  • Configuring Forced User Actions
  • Configuring Forced User Actions using WebStation
  • Adding a Checklist to an Alarm
  • Adding a Checklist to an Alarm using WebStation
  • Editing a Checklist
  • Editing a Checklist using WebStation
  • Creating a Checklist
  • Creating a Checklist using WebStation
  • Import and Export of Supporting Objects