earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Enterprise Central, Enterprise Server, FDP Server
Functionalities: Trends
12/3/2024

Create Trend Log Wizard – Configure Change of Value Trend Log Page

Use the Configure Change of Value Trend Log page to configure the settings of a change of value trend log.

 
action_zoom_plus_stroke Configure Change fof Value Trend Log page
Figure: Configure Change fof Value Trend Log page

Table: Configure Change of Value Trend Log Page

Component

Description

Logged variable

Enter the variable that you want to log.

 
action_zoom_plus_stroke

Set unit

Click to open the Unit Selection dialog box where you select the unit. For more information, see Select Unit Dialog Box .

Delta

​Select the minimum value change that triggers a new record.

Activation variable

Enter the variable that is to start the trend log.

Activation time

​Type the start time of the trend log.

Maximum log interval

Select the maximum time that can pass between two recordings regardless of whether the delta value has been exceeded or not.

Log size

Select the number of records to store before old records are overwritten including internal records generated by the trend.

Available trend storage

Displays the trend storage usage and the number of records left in the trend storage.

Clear when enabled

​Select True to clear the trend log when it is enabled.

  • Change of Value Trend Logs
  • Change of Value Trend Log Properties – Basic Tab
  • Select Unit Dialog Box
  • Trend Units
  • Trend Log Activation
  • Log Record Storage
  • Create Object Dialog – Naming the Object Page