earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WorkStation
Functionalities: Basic Functionality
12/10/2024

Logging on to WorkStation as an EcoStruxure Building Operation User

You log on to WorkStation to securely access the functions in the EcoStruxure BMS.

Important:

​​Ensure that you have a working and available WorkStation license. A working license is required to log on to WorkStation.

Show More
action_close

You log on to WorkStation or WebStation to securely access the EcoStruxure BMS features.

Log on to WorkStation

You log on to WorkStation with your current Windows credentials, as another Windows user, or as an EcoStruxure BMS user. Your system administrator decides which type of user you log on as. ​

To log on to WorkStation using an EcoStruxure BMS account, you need to know the following account information:

  • User name

  • Password

  • Domain

  • EcoStruxure BMS server

To log on to WorkStation using a Windows account, you need to know the EcoStruxure BMS server.

The account information for both the EcoStruxure BMS account and the Windows account is provided by the system administrator.

Important:

​​Ensure that you have a working and available WorkStation license. A working license is required to log on to WorkStation.

Remember me on this computer

For a faster log on in Workstation, use the Remember me feature to automatically fill in your user name, password, domain and server. Both BMS users and Windows users can use the Remember me feature.

Add a display name of the server address

When you log on to a new server, its IP address is added to the server list. You can add a display name of the server address to make it easier to find your server in the list.

Log on to WebStation

To log on to WebStation, you need to know the following account information:

  • User name

  • Password

  • Domain

  • EcoStruxure BMS server

The account information for your account is provided by the system administrator.

To log on to WorkStation as an EcoStruxure Building Operation user
  1. In the User name box, type the EcoStruxure Building Operation user name.

  2. In the Password box, type the password.

  3. In the Domain box, type a domain name. If you do not enter a domain name, you are logged on to the local domain.

  4. Select the Server hypertext transfer protocol option for communication with the EcoStruxure BMS server.

  5. In the Server box, enter an EcoStruxure BMS server name or an IP address.

    Note:

    You can also, in the scroll down menu, choose a server host name from the list. When you start typing the host name or the IP number of the server, you will be offered suggestions from the saved list.

    Note:

    When you log on to a new server, its IP address is added to the server list. You can add a display name of the server address to make it easier to find your server in the list.

  6. Select Remember me to have WorkStation remember your settings.

  7. Click Log on .

  8. You can register the system now or later:

    • Click Register now to register your system. For more information, see System Registration .

    • Click Register later to skip registration and register at a later time.

  9. If the Select Default Workspace window is displayed, click the workspace you want to have as the default.

  • Log on to WorkStation or WebStation
  • Logging on to WorkStation using your Windows user account
  • Logging on to WorkStation as another Windows User
  • Saving Log On Details
  • Workspaces
  • Selecting a Default Workspace
  • Switching Workspaces
  • Logging Off WorkStation
  • Exiting WorkStation
  • Changing Your Password
  • Building Operation WorkStation Window
  • System Registration
  • Online Registration
  • Registering an Online System
  • Offline Registration
  • Registering an Offline System