You log on to WorkStation or WebStation to securely access the EcoStruxure BMS features.
Important:
What you can see and which tasks you can perform depend on the software permissions based on your role in the EcoStruxure BMS.
WebStation Login
To log on to WebStation, you need to know the following account information:
User name
Password
Domain
EcoStruxure BMS server
The account information for your account is provided by the system administrator.
You log on to WorkStation with your current Windows credentials, as another Windows user, or as an EcoStruxure BMS user. Your system administrator decides which type of user you log on as.
To log on to WorkStation using an EcoStruxure BMS account, you need to know the following account information:
User name
Password
Domain
EcoStruxure BMS server
To log on to WorkStation using a Windows account, you need to know the EcoStruxure BMS server.
The account information for both the EcoStruxure BMS account and the Windows account is provided by the system administrator.
Remember me on this computer
For a faster log on in Workstation, use the Remember me feature to automatically fill in your user name, password, domain and server. Both BMS users and Windows users can use the Remember me feature.
Add a display name of the server address
When you log on to a new server, its IP address is added to the server list. You can add a display name of the server address to make it easier to find your server in the list.