1017 Topic(s)
You perform the following steps to power up an RP-C 230 V controller model.
You install an RP controller expansion Insight-Sensor on an octagon junction box using the supplied mounting ring to properly fasten the Insight-Sensor to the junction box.
You install an RP controller expansion Insight-Sensor on a ceiling using the supplied mounting ring to properly fasten the Insight-Sensor on the ceiling.
You install an RP controller expansion Insight-Sensor into a dropped ceiling using the mounting springs to properly fasten the Insight-Sensor to a ceiling tile.
You connect RP controller expansion modules and multi-sensors to the RP-C room bus to provide the devices with power and communication from the RP-C controller.
You create an extended trend log to store log records for a longer period of time and free up memory in the automation server.
You log on to WorkStation to securely access the functions in the EcoStruxure BMS.
You edit a backup rule on an EcoStruxure BMS server to change the type of data that you want to back up. You can also set up this backup rule to follow a shadow schedule that references a lead schedule managed on another EcoStruxure BMS server.
You create an out of reference range alarm to trigger an alarm when a variable, such as a temperature, differs from a reference value.
You create an out of range alarm to trigger an alarm when a variable, such as a temperature, is not within its specified range.