earth_america
user_standard Log on
action_search_stroke
earth_america

Builder View

Refine your search
arrow2_down
Refine your search
Ok
Ok
Ok

11 Topic(s)

Concept

On Canvas in Builder View live mode, you display your canvas objects to be able to see the exposed source and target properties for the objects.

User Interface

Use the canvas binding context menu, when a binding on the canvas is selected, to select the binding in the Bindings view list or to select a type of visual style of the binding between canvas objects.

User Interface

Use the Builder View toolbar to navigate between different canvas views or to change the canvas zoom level.

User Interface

Use the Bindings view to see all local and external bindings between canvas objects.

Concept

In Builder View, the canvas objects are designed to make the configuration of the objects seamless. Canvas objects are displayed visually on the Builder View canvas.

Concept

The canvas in Builder View displays objects that are located inside the selected folder structure in the system tree, or objects outside the selected folder structure, which are bound to objects inside the selected folder structure, and also bindings between the canvas objects. The bound canvas objects have exposed property names that are displayed as binding ports.

Concept

Builder View is a graphic binding and engineering tool, which allows users of EcoStruxure BMS to graphically view bindings on a canvas between canvas objects properties, and to monitor and follow data flows. Builder View displays objects that are located in the selected current folder structure, and also displays objects outside the current folder structure that are bound to objects within the current folder structure. The bound canvas objects have exposed property names that are displayed as binding ports.

Concept

Many of the Builder View Live Mode commands can be accessed using keyboard and mouse shortcuts.

Concept

Bindings in Builder View are connections between two or more variables for data exchange. In its simplest form, the binding consists of a source and a target. The source supplies the value to the target.

Concept

In Builder View Live Mode, you display your canvas objects to be able to see the exposed source and target properties for the objects.