earth_america
user_standard Log on
action_search_stroke
earth_america

RP-C

Refine your search
arrow2_down
Refine your search
Ok
Ok
Ok

266 Topic(s)

Concept

The Commission mobile application is a powerful and convenient tool for use with BACnet/IP Controller devices. However, as with any application, security considerations and appropriate actions must be taken to guard against unauthorized access.

Concept

You download an Application Image that contains a Configuration Menu to a BACnet/IP controller to configure a device. Use this workflow to implement the Configuration Menu using the Commission mobile application. Related information can be found in the section after the flowchart.

How to

You test a 0-10V light module output to ensure it is operating correctly.

How to

You can use the Controller List Creator function of the Commission mobile application to capture device information from the Digital Matrix symbol on the tear-off product info labels of BACnet/IP devices.

How to

You can use the Commission mobile application to update or delete your Schneider Electric Identity Management System (IDMS) user profile on the Schneider Electric Exchange site.

How to

The Browse Objects function of the Commission mobile application creates a list of all the objects within a BACnet/IP controller. You can use this function to view and, if needed, edit the properties of any of these objects.

How to

You change the PIN of the SpaceLogic Bluetooth Adapter for best security practices. The Bluetooth Adapter PIN is engineered to a default code of 333666 and should be changed to a secure code before you perform device commissioning. You configure the password for Bluetooth access in the RP controller.

How to

You calibrate a high or low voltage blind power module because blinds come in all shapes and sizes, as do the windows that they are fixed to. Out of the box, the RP-C controller blind module does not know the size of the window or the blind. As a result, the controller cannot determine how long the motor should spin in order to configure the blind at 50% and the angle at 25%, for example.

How to

You test the SMI blind outputs to ensure that the blinds are operating properly.

How to

In the Project List view of the Controller List Creator function, you can view existing projects and delete or create new ones.