The SEBOX483212 enclosure is a 11.8 in (300 mm) deep box. Its features include a reversible door with invisible hinges that open 120 degrees, a standard 3mm double bar lock with screw driver lock feature and a foamed-in polyurethane gasket door that prevents water and dust migration. An optional key lock is also available. You can order the enclosures with an optional perforated back plate using the P suffix on the model. The SEBOX483212 is designed for use with EcoStruxure Building Operation components, such as Automation Servers, Power Supplies, MP-X IP controllers and Input/Output modules.
The SEBOX483212 is a wall-mounted enclosure with the following dimensions:
Height: 47.2 inch (1200 mm)
Width: 31.5 inch (800 mm)
Depth: 11.8 inch (300 mm)
Cubic inch volume: 17544 (288000 cu. cm)
For more information, see Mounting a UL 864 Smoke Control Enclosure .
Should you want more information on this or any other SEBOX enclosure, the datasheets, installation sheets, and other relevant documentation are available at the following URL:
http://www.se.com/us/en/
Access that page and then search on the NSYCRNxxxxx part numbers and the SEBOX model numbers to which they correlate as shown in the table that follows:
|
NSYCRNxxxxx Part Number |
SEBOX Model |
|
NSYCRN345150 |
SEBOX121806 |
|
NSYCRN44200 |
SEBOX161608 |
|
NSYCRN55250 |
SEBOX202010 |
|
NSYCRN66200 |
SEBOX242408 |
|
NSYCRN106250 |
SEBOX392410 |
|
NSYCRN108250 |
SEBOX393210 |
|
NSYCRN108300 |
SEBOX483212 |