earth_america
user_standard Accedi
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concetto

Concetto


Prodotti: MP-V
Funzionalità: Hardware
Versione del prodotto: 2022, 2023, 2024, 7.0
30/11/2023

MP-V Models

The MP-V comes in two models with a different I/O point count and different I/O point mix.

Per maggior informazioni, consulta MP-V Onboard I/O .

Model

I/O Points

MP-V-7A a

7

MP-V-9A a

9

  1. This model is available in a Buy American Act (BAA) compliant variant, which has the suffix “-BAA” in the name. For more information, see the SpaceLogic MP-V Pro Specification Sheet. The BAA compliant variant does not differ in terms of hardware and functionality.

The MP-V-7A and MP-V-9A have the same compact design and dimensions as a majority of the Schneider Electric VAV controller models from Andover Continuum, TAC Vista, and TAC I/A Series product lines. You can use the MP-V-7A and MP-V-9A for both cooling and heating applications.

Per maggior informazioni, consulta MP-V Onboard I/O .

Differences Between MP-V Hardware Versions

There are few differences in hardware between different hardware versions of the MP-V models.

Per maggior informazioni, consulta Differences Between MP-V Hardware Versions .

  • Hardware Overview
  • MP-C Controllers
  • MP-V Onboard I/O
  • SpaceLogic MP-V
  • Differences Between MP-V Hardware Versions