earth_america
user_standard Connexion
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Comment faire pour

Comment faire pour


Produits : eCommission SmartX Controllers, IP-IO , MP-C, MP-V, RP-C
Fonctionnalités : Ingénierie, Dispositifs SmartX IP Controller
Version produit : 3.3, 2022, 2023, 2024, 7.0
18/07/2021

Downloading and Starting the eCommission SmartX Controllers Mobile Application

You download and start the eCommission SmartX Controllers mobile application to perform commissioning, flow balance, and checkout operations on BACnet/IP controllers.

Afficher plus
action_close

Prior to using the eCommission SmartX Controllers mobile application at a job site, there are some preparations you must make to facilitate device commissioning.

Pour plus d'informations, voir Présentation de l'application mobile Commission .

Launching and Activating the eCommission Application

You launch and then activate the eCommission SmartX Controllers mobile application to create an account before you can perform any tasks.

Downloading and Starting the eCommission Application

You download and start the eCommission SmartX Controllers mobile application to perform commissioning, flow balance, and checkout operations on BACnet/IP controllers.

Pour plus d'informations, voir Downloading and Starting the eCommission SmartX Controllers Mobile Application .

Transferring an Application Image File to a Mobile Device

Image files are created by a WorkStation user and contain pre-engineered objects, properties, and values. Download an Image to a BACnet/IP controller to facilitate device commissioning tasks.

Pour plus d'informations, voir Image Downloading .

To download and start the eCommission SmartX Controllers mobile application
  1. Download and then install the eCommission SmartX Controllers application to the mobile device or Windows 10 laptop from Google Play, the Apple App Store, or the Microsoft Store.

    Déclaration

    eCommission SmartX Controllers is the name of the application used in the download sources.

  2. From your mobile device or Windows 10 laptop, start the eCommission application.

  3. In the Login view, in the Username box, type your username.

  4. In the Password box, type your password.

  5. Select Log on .

Now you can use the eCommission application to connect to BACnet/IP controllers.

  • Preparations
  • Flux de travail de technicien pour l'application eCommission
  • Electrician Workflow for the eCommission Application
  • Flux de travail de l'équilibreur de débit