earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Poradnik

Poradnik


Produkty: eCommission SmartX Controllers, IP-IO , MP-C, MP-V, RP-C
Funkcje: Inżynieria, Urządzenia SmartX IP Controller
Wersja produktu: 3.3, 2022, 2023, 2024, 7.0
2021-07-18

Downloading and Starting the eCommission SmartX Controllers Mobile Application

You download and start the eCommission SmartX Controllers mobile application to perform commissioning, flow balance, and checkout operations on BACnet/IP controllers.

Pokaż więcej
action_close

Prior to using the eCommission SmartX Controllers mobile application at a job site, there are some preparations you must make to facilitate device commissioning.

Więcej informacji zawiera Commission Mobile Application Overview .

Launching and Activating the eCommission Application

You launch and then activate the eCommission SmartX Controllers mobile application to create an account before you can perform any tasks.

Downloading and Starting the eCommission Application

You download and start the eCommission SmartX Controllers mobile application to perform commissioning, flow balance, and checkout operations on BACnet/IP controllers.

Więcej informacji zawiera Downloading and Starting the eCommission SmartX Controllers Mobile Application .

Transferring an Application Image File to a Mobile Device

Image files are created by a WorkStation user and contain pre-engineered objects, properties, and values. Download an Image to a BACnet/IP controller to facilitate device commissioning tasks.

Więcej informacji zawiera Image Downloading .

To download and start the eCommission SmartX Controllers mobile application
  1. Download and then install the eCommission SmartX Controllers application to the mobile device or Windows 10 laptop from Google Play, the Apple App Store, or the Microsoft Store.

    Uwaga

    eCommission SmartX Controllers is the name of the application used in the download sources.

  2. From your mobile device or Windows 10 laptop, start the eCommission application.

  3. In the Login view, in the Username box, type your username.

  4. In the Password box, type your password.

  5. Select Log on .

Now you can use the eCommission application to connect to BACnet/IP controllers.

  • Preparations
  • Technician Workflows for eCommission Application
  • Electrician Workflow for the eCommission Application
  • Flow Balancer Workflow