The eCommission Bluetooth Adapter is plugged into a SmartX Sensor to provide a wireless Bluetooth connection to the SmartX IP controller (Sensor Bus compliant controller) for commissioning, maintenance, and troubleshooting of the controller and the sensor.
The eCommission Bluetooth Adapter provides a bridge between a Bluetooth enabled mobile device running the eCommission SmartX Controllers mobile application and the Sensor Bus on the SmartX IP controller. The eCommission mobile application is used to perform commissioning, flow balance, and checkout operations on SmartX IP controllers. Para obtener más información, consulte Resumen de la aplicación móvil eCommission SmartX Controllers .
The Bluetooth adapter is designed to be connected to a SmartX Sensor, which in turn is connected to the Sensor Bus port on the SmartX IP controller. The Bluetooth adapter cannot be connected directly to the Sensor Bus port on the SmartX IP controller. Para obtener más información, consulte SmartX IP Controller Sensor Bus .
The Bluetooth adapter is plugged into a connector on the upper-right side of the SmartX Sensor. Para obtener más información, consulte Installing eCommission Bluetooth Adapter on a SmartX Sensor . The physical connector on the sensor is a USB style connector, but the electrical interface and communication protocol are not USB. The Bluetooth adapter communicates with the SmartX IP controller over the Sensor Bus using the RS-485 physical layer.
The Bluetooth adapter PCB has a card-edge connector that protrudes from the PCB and mates with the SmartX Sensor connector.
The Bluetooth adapter is powered by the SmartX Sensor, which also provides transient protection to the adapter.
The Bluetooth adapter is housed in a plastic enclosure, which has a protective cap to help protect the PCB card edge when the adapter is not connected to a SmartX Sensor. The protective cap has a hinge mechanism. The cap can either hang down, or rotate to the back end and snap on, when the adapter is connected to a SmartX Sensor. The adapter is delivered with a lanyard that can be attached to a loop on the protective cap. Para obtener más información, consulte Attaching a Lanyard to eCommission Bluetooth Adapter .
The Bluetooth adapter has a momentary push-button switch that is used for pairing the adapter with a mobile device running the eCommission SmartX Controllers mobile application. Para obtener más información, consulte Conectarse a un controlador con el adaptador Bluetooth .The Bluetooth adapter sends out a unique signal that enables the mobile device to pair with the correct adapter. A blue indicator LED on the adapter indicates the status.
LED Patterns |
Condition/Mode |
Blue, flashing (2 s ON, 8 s OFF) |
Default Mode (No Bluetooth client connection, no SmartX IP controller connection) |
Blue, flashing (1 s ON, 1 s OFF) |
Advertising Mode (No Bluetooth client connection, no SmartX IP controller connection, connection is possible) |
Blue, constant (always ON) |
Connected Mode (Bluetooth client connection, no SmartX IP controller connection) |
Blue, ON when transmitting, OFF otherwise |
Active Mode (Bluetooth client connection, SmartX IP controller connection active) |
Blue, flashing (2 s ON, 6 s OFF, 8 s ON, 4 s OFF) |
DFU Mode (Waiting for user to press and hold push-button) |
Electrical | |
DC input power consumption
|
Maximum 0.25 W
|
DC input supply voltage
|
5.0 to 5.5 VDC (powered by the SmartX Sensor)
|
Communications | |
Wireless communications
|
Bluetooth
®
4.2 Low Energy compliant
|
Bluetooth
®
5 Advertising
|
|
Frequency: 2.4 GHz
|
|
Line-of-sight range: max. 50 m (164 ft)
|
|
SmartX communications
|
RS-485, proprietary Sensor Bus protocol
|
Operation environment | |
Ambient temperature, operating
|
0 to 50 °C (32 to 122 °F)
|
Ambient temperature, storage
|
-40 to +70 °C (-40 to +158 °F)
|
Humidity
|
Maximum 95 % RH non-condensing
|
Mechanical | |
Dimensions
|
70 W x 32 H x 12 D mm (2.8 W x 1.3 H x 0.5 D in.)
|
Weight
|
0.02 kg (0.05 lb) with lanyard
|
Hardware | |
CPU type
|
ARM Cortex-M4 single-core
|
Frequency
|
38.4 MHz
|
SRAM (embedded)
|
32 KB
|
Flash memory (embedded)
|
256 KB
|
Flash memory (serial)
|
1 MB
|
Status indicator
|
LED (blue)
|
Button
|
Momentary push-button switch
|