Running the eCommission SmartX Controllers mobile application on a Windows laptop computer, you can connect directly to a BACnet/IP controller by Ethernet wire. Optionally, you can use an Ethernet switch to connect the computer and the BACnet/IP controller.
Configure the network connections on the eCommission application computer and the BACnet/IP controller for DHCP addressing.
Pour plus d'informations, voir Configuring BACnet/IP Device Settings .
Connect an Ethernet cable between the eCommission application computer and Port 1 of the BACnet/IP controller. If you are using an Ethernet switch, connect the computer and the controller to the switch, using Ethernet cables.
Because an actual DHCP server is not used, both the eCommission application computer and the BACnet/IP controller will self-assign link-local IP addresses.
In the eCommission application, on the Select Connection view, select the WiFi icon
In the Device List view, select the BACnet/IP controller to make the connection.
Using the eCommission application, you can now perform tasks on the connected BACnet/IP controller as needed.