earth_america
user_standard Connexion
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Comment faire pour

Comment faire pour


Produits : eCommission SmartX Controllers, MP-C, MP-V, SmartX Sensor
Fonctionnalités : Matériel
Version produit : 3.0, 3.1, 3.2
13/07/2019

Attaching a Lanyard to eCommission Bluetooth Adapter

You attach a lanyard to eCommission Bluetooth Adapter to help keeping the adapter securely on your wrist and to help preventing loss of the adapter.

Déclaration

The lanyard is delivered with the adapter.

Afficher plus
action_close

The eCommission Bluetooth Adapter is plugged into a SmartX Sensor to provide a wireless Bluetooth connection to the SmartX IP controller (Sensor Bus compliant controller) for commissioning, maintenance, and troubleshooting of the controller and the sensor.

Déclaration

SMARTX SENSOR OR OTHER EQUIPMENT DAMAGE

  • Plug in the adapter with the button to the front.

  • Do not plug into any device other than a SmartX Sensor.

Failure to follow these instructions can result in equipment damage.

 
action_zoom_plus_stroke  eCommission Bluetooth Adapter provides Bluetooth access to SmartX IP controllers
Figure : eCommission Bluetooth Adapter provides Bluetooth access to SmartX IP controllers

The eCommission Bluetooth Adapter provides a bridge between a Bluetooth enabled mobile device running the eCommission SmartX Controllers mobile application and the Sensor Bus on the SmartX IP controller. The eCommission mobile application is used to perform commissioning, flow balance, and checkout operations on SmartX IP controllers. Pour plus d'informations, voir Vue d'ensemble de l'application mobile eCommission SmartX Controllers .

The Bluetooth adapter is designed to be connected to a SmartX Sensor, which in turn is connected to the Sensor Bus port on the SmartX IP controller. The Bluetooth adapter cannot be connected directly to the Sensor Bus port on the SmartX IP controller. Pour plus d'informations, voir SmartX IP Controller Sensor Bus .

The Bluetooth adapter is plugged into a connector on the upper-right side of the SmartX Sensor. Pour plus d'informations, voir Installing eCommission Bluetooth Adapter on a SmartX Sensor . The physical connector on the sensor is a USB style connector, but the electrical interface and communication protocol are not USB. The Bluetooth adapter communicates with the SmartX IP controller over the Sensor Bus using the RS-485 physical layer.

The Bluetooth adapter PCB has a card-edge connector that protrudes from the PCB and mates with the SmartX Sensor connector.

The Bluetooth adapter is powered by the SmartX Sensor, which also provides transient protection to the adapter.

The Bluetooth adapter is housed in a plastic enclosure, which has a protective cap to help protect the PCB card edge when the adapter is not connected to a SmartX Sensor. The protective cap has a hinge mechanism. The cap can either hang down, or rotate to the back end and snap on, when the adapter is connected to a SmartX Sensor. The adapter is delivered with a lanyard that can be attached to a loop on the protective cap. Pour plus d'informations, voir Attaching a Lanyard to eCommission Bluetooth Adapter .

 
action_zoom_plus_stroke eCommission Bluetooth Adapter
Figure : eCommission Bluetooth Adapter

The Bluetooth adapter has a momentary push-button switch that is used for pairing the adapter with a mobile device running the eCommission SmartX Controllers mobile application. Pour plus d'informations, voir Connexion à un contrôleur via l'adaptateur Bluetooth .The Bluetooth adapter sends out a unique signal that enables the mobile device to pair with the correct adapter. A blue indicator LED on the adapter indicates the status.

Table : eCommission Bluetooth Adapter LED Patterns

LED Patterns

Condition/Mode

Blue, flashing (2 s ON, 8 s OFF)

Default Mode (No Bluetooth client connection, no SmartX IP controller connection)

Blue, flashing (1 s ON, 1 s OFF)

Advertising Mode (No Bluetooth client connection, no SmartX IP controller connection, connection is possible)

Blue, constant (always ON)

Connected Mode (Bluetooth client connection, no SmartX IP controller connection)

Blue, ON when transmitting, OFF otherwise

Active Mode (Bluetooth client connection, SmartX IP controller connection active)

Blue, flashing (2 s ON, 6 s OFF, 8 s ON, 4 s OFF)

DFU Mode (Waiting for user to press and hold push-button)

Spécifications

Electrical
DC input power consumption
Maximum 0.25 W
DC input supply voltage
5.0 to 5.5 VDC (powered by the SmartX Sensor)
Communications
Wireless communications
Bluetooth ® 4.2 Low Energy compliant
  
Bluetooth ® 5 Advertising
  
Frequency: 2.4 GHz
  
Line-of-sight range: max. 50 m (164 ft)
SmartX communications
RS-485, proprietary Sensor Bus protocol
Operation environment
Ambient temperature, operating
0 to 50 °C (32 to 122 °F)
Ambient temperature, storage
-40 to +70 °C (-40 to +158 °F)
Humidity
Maximum 95 % RH non-condensing
Mechanical
Dimensions
70 W x 32 H x 12 D mm (2.8 W x 1.3 H x 0.5 D in.)
Weight
0.02 kg (0.05 lb) with lanyard
Hardware
CPU type
ARM Cortex-M4 single-core
Frequency
38.4 MHz
SRAM (embedded)
32 KB
Flash memory (embedded)
256 KB
Flash memory (serial)
1 MB
Status indicator
LED (blue)
Button
Momentary push-button switch

To attach a lanyard to eCommission Bluetooth Adapter
  1. Thread the thin loop of string at the end of the lanyard through the loop on the protective cap of the adapter.

     
    action_zoom_plus_stroke
  2. Thread the lanyard (larger loop) through the smaller loop.

     
    action_zoom_plus_stroke
  3. Pull the lanyard to tighten the loop and secure the lanyard to the adapter's protective cap.

     
    action_zoom_plus_stroke
  • eCommission Bluetooth Adapter
  • Installing eCommission Bluetooth Adapter on a SmartX Sensor