earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AS-B, Device Administrator, ​License Administrator, AS-P
Functionalities: Hardware, SmartDrivers
Product version: 3.3
12/17/2021

Automation Server Licensing Workflow

Use this workflow to add licenses to automation servers using Device Administrator.

Related information can be found in the sections after the flowchart.

 
action_zoom_plus_stroke Automation Serverr licensing workflow
Figure: Automation Serverr licensing workflow
Add Entitlements to Device Administrator

In Device Administrator, add an Entitlement that contains products and licenses to Device Administrator.

For more information, see Adding an Entitlement to Device Administrator .

Assign licenses to an automation server

Assign the licenses in the Entitlement for the features you want to use on the automation servers.

For more information, see Assigning Licenses .

Activate licenses on an automation server

For more information, see Activating Licenses Online .

If you do not have internet access, you can activate licenses offline.

For more information, see Offline Activation of Licenses Workflow .

Important:

Activated licenses cannot be deactivated.

  • Automation Server Licensing Overview
  • Adding an Entitlement to Device Administrator
  • Assigning Licenses
  • Activating Licenses Online
  • Offline Activation of Licenses Workflow