earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: AS-B, Device Administrator, ​License Administrator, AS-P
Functionalities: Hardware, SmartDrivers
Product version: 3.3
7/23/2021

Activating Licenses Online

You activate licenses so that you can access the features.

Show More
action_close

Device Administrator is used to manage licenses on automation servers.

Licenses on Automation Servers

The following features of an automation server need licenses.

SmartDrivers

To be able to use SmartDrivers on an automation server one license is needed for every SmartDriver that runs on the automation server.

SNMP Notifications

To be able to use SNMP Notification on an automation server, a license is required.

For a stand-alone automation server, the license can be local for the automation server and administered by Device Administrator.

In a multi-server system, you can use inherited licenses.

For more information, see Inherited Licenses .

Personal Dashboards

To be able to create personal dashboards on an automation server, you need a license. Personal dashboards are used in WebStation.

For a stand-alone automation server, the license can be local for the automation server and administered by Device Administrator.

In a a multi-server system, you can use inherited licenses.

For more information, see Inherited Licenses .

TimescaleDB

To be able to use TimescaleDB on an automation server, a license is required.

For more information, see Inherited Licenses .

Entitlements, Products, and Licenses

Licenses are bought as products and delivered in Entitlements. An Entitlement is a container that can contain several products. The products contain the licenses and they can differ in quantity and contents.

Automation Server Licensing Workflow

Use this workflow to add licenses to automation servers using Device Administrator.

For more information, see Automation Server Licensing Workflow .

Certificates

It is recommended to use HTTPS for the communication between Device Administrator and automation servers when you manage licenses.

For more information, see Certificates in Device Administrator .

Important:

Activated licenses cannot be deactivated.

To activate licenses online
  1. In Device Administrator, click Servers .

  2. Select Show licenses .

  3. Select the automation servers where you want to activate the licenses.

  4. Click Activate licenses .

  5. Click Online .

  6. In the Activate Licenses dialog box, click OK .

  7. In the Detailed Progress dialog box, view the progress of the activation.

All assigned licenses are now activated.

  • Automation Server Licensing Overview
  • Automation Server Licensing Workflow
  • Offline Activation of Licenses Workflow
  • Activate Licenses Dialog Box
  • Assigning Licenses
  • Detailed Progress Dialog Box