There is one or more LEDs on the front panel of the RP controller expansion modules.
Function |
Color |
Status (RP controller expansion module) |
Red, Green |
Light Status a |
Green |
Blind Status |
Green |
Relay Status b |
Green |
The LEDs indicate the status of the RP controller expansion module and the status of the relays or motor drivers used for controlling the power distribution to the lights and blinds.
The RP controller expansion module Status LED can be configured in the following modes:
Show status mode
Off mode
You configure the Status LED mode in the EcoStruxure Building Operation software. Więcej informacji zawiera Configuring RP Controller Expansion Modules .
The RP controller expansion module Status LED indicates the condition of the device.
LED Patterns |
Condition |
Recommended action |
Green, constant |
Normal operation, status OK. |
No action required. |
Green constant, with red flash (100 ms every 2 seconds) |
Normal operation, status OK. However, the RP controller expansion module has detected and logged an abnormal condition. When the RP-C has retrieved the diagnostics from the module, the Status LED returns to constant green light. Więcej informacji zawiera RP Controller Expansion Module Diagnostics . |
No action required. |
Green, flashing (~1 Hz) |
Device is starting or restarting.
|
No action required. |
Green, flashing medium (~2 Hz) |
Device is in maintenance mode. Więcej informacji zawiera RP Controller Expansion Module Maintenance Modes . |
To exit the maintenance mode, configure a unique device address in the range supported by the RP-C controller model and then reset the device by disconnecting and reconnecting the device to the RP-C room bus. Więcej informacji zawiera Configuring the Room Bus Address for an RP Controller Expansion Module .Więcej informacji zawiera Connecting RP Controller Expansion Modules to an RP Controller . |
Green, flashing fast (~5 Hz) |
Device is initializing. |
No action required. |
Red, flashing (~1 Hz) |
Device is non-operational due to a detected error. Device is forced into maintenance mode. |
Contact Schneider Electric Product Support Services for assistance. |
Red, flashing fast (~5 Hz) |
Device is inoperable due to a detected, non-recoverable error. |
Contact Schneider Electric Product Support Services for assistance or return the device to Schneider Electric. |
Red, constant |
Device is inoperable due to a detected, non-recoverable error. |
Return the device to Schneider Electric. |
The RP controller expansion module Status LED is disabled.
The Light Status LEDs indicate the condition of the light output relays, which control the power distribution (230 VAC from the power supply) to the lights. The LEDs are available on RP controller expansion light modules with power distribution capability.
LED Patterns |
Condition |
Recommended action |
Green, constant |
Light output relay is active (energized), power distribution to the light is enabled. |
No action required. |
The Blind Status LEDs indicate the condition of the blind output relays, which control the power distribution (230 VAC from the power supply) to the blind motors.
LED Patterns |
Condition |
Recommended action |
Green, constant |
Blind output relay is active (energized), power distribution to the blind motor is enabled. |
No action required. |
The Blind Status LEDs indicate the condition of the blind output motor drivers, which control and drive the blind motors.
LED Patterns |
Condition |
Recommended action |
Green, constant |
Blind output motor driver is active. |
No action required. |
The Relay Status LEDs indicate the condition of the output relays, which control the power distribution (100 to 277 VAC from the power supply) to the lights.
LED Patterns |
Condition |
Recommended action |
Green, constant |
Output relay is active (energized), power distribution to the light is enabled. |
No action required. |