earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Pojęcie

Pojęcie


Produkty: CRS-HH-REL-10, RP-C, RP-C-EXT-0-10V-4, RP-C-EXT-0-10V-4-PD, RP-C-EXT-BL-2-LV-PD, RP-C-EXT-BL-4-HV-PD, RP-C-EXT-BL-SMI-2-LV-PD, RP-C-EXT-BL-SMI-4-HV-PD, RP-C-EXT-DALI, RP-C-EXT-DALI-M-PD, RP-C-EXT-IS-BLE, RP-C-EXT-MS-BLE, RP-C-EXT-REL-4
Funkcje: Sprzęt
Wersja produktu: 2022, 2023, 2024, 7.0
2024-03-06

RP Controller Expansion Modules

arrow1_rotationLight Modules arrow1_rotationBlind Modules arrow1_rotationRelay Modules arrow1_rotationSensor Modules arrow1_rotationRemote Control

The RP controller expansion modules provide a range of devices that can be combined to form a connected room solution. The RP controller expansion modules are connected to the RP controller room bus and provide the RP controllers with I/O expansion and sensors that enable lighting and blind control.

The software application for lighting and blind control runs in the RP controller. There is typically one RP controller per room, but some RP controller models support control of up to four rooms per controller. Więcej informacji zawiera RP-C Models .. The RP controllers are connected to an automation server, which controls and manages all the RP controllers. There is typically one automation server per floor. The automation servers are in turn typically connected to an Enterprise Server.

 
action_zoom_plus_stroke RP controller expansion modules for a connected room solution
Rysunek: RP controller expansion modules for a connected room solution

The RP controllers can use input data from SpaceLogic Sensor devices to control the lighting and blinds. The SpaceLogic Sensor devices are connected to the RP controller sensor bus. The SpaceLogic Sensor devices provide sensors for temperature, humidity, CO 2 , and occupancy in a room. SpaceLogic Sensor models with touchscreen display enable users to adjust the lighting and blinds in a room. Więcej informacji zawiera SpaceLogic Sensors - SXWS Sensors for MP and RP IP Controllers - Specification Sheet .

In addition, the EcoStruxure Building Engage mobile application allows building occupants to adjust the room comfort settings (room temperature, fan speed, lighting, and window blinds) using a smartphone connected to the RP controller through Bluetooth Low Energy. Więcej informacji zawiera Engage .

Light Modules

The RP controller expansion light modules enable control of lights with electrical ballasts and LED drivers.

Więcej informacji zawiera Light Modules .

Blind Modules

The RP controller expansion blind modules enable control of motorized window blinds and shutters.

Więcej informacji zawiera Blind Modules .

Relay Modules

The RP controller expansion relay modules enable control of lights and motorized window blinds and shutters.

Więcej informacji zawiera Relay Modules .

Sensor Modules

The RP controller expansion sensor modules can be used, for example, for infrared motion detection and luminosity measurement.

Więcej informacji zawiera Sensor Modules .

Remote Control

The RP-C-RC-BLE remote control connects wirelessly to the RP controller expansion sensor module, such as the Multi-sensor and Insight-Sensor, and enables the occupants of modern office buildings to control the comfort level of their space.

Więcej informacji zawiera RP-C-RC-BLE .

  • Hardware Overview
  • RP-C Models
  • Engage
  • Light Modules
  • Blind Modules
  • Relay Modules
  • Sensor Modules
  • RP-C-RC-BLE