earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Pojęcie

Pojęcie


Produkty: RP-C, RP-C-EXT-IS-BLE, RP-C-EXT-MS-BLE
Funkcje: Sprzęt
Wersja produktu: 2022, 2023, 2024, 7.0
2022-04-05

RP Controller Expansion Sensor Module LED

arrow1_rotationStatus LED

There is one LED on the RP controller expansion sensor modules. The LED is integrated with the Set button.

 
action_zoom_plus_stroke Sensor module LED
Rysunek: Sensor module LED

Tabela: Sensor Module LED

Function

Color

Status

Red, Green

Status LED

The sensor module Status LED can be configured in the following modes:

  • Show status mode

  • Off mode

You configure the Status LED mode in the EcoStruxure Building Operation software. Więcej informacji zawiera Configuring RP Controller Expansion Modules .

Show status mode

The sensor module Status LED indicates the condition of the device.

Tabela: Sensor Module Status LED Patterns

LED Patterns

Condition

Recommended action

Green, constant

Normal operation, status OK.

No action required.

Green constant, with red flash (100 ms every 2 seconds)

Normal operation, status OK.

However, the sensor module has detected and logged an abnormal condition. When the RP-C has retrieved the diagnostics from the sensor module, the Status LED returns to constant green light. Więcej informacji zawiera RP Controller Expansion Module Diagnostics .

No action required.

Green, flashing (~1 Hz)

Device is starting or restarting.

No action required.

Green, flashing medium (~2 Hz)

Device is in maintenance mode. Więcej informacji zawiera RP Controller Expansion Module Maintenance Modes .

To exit the maintenance mode, configure a unique device address in the range supported by the RP-C controller model and then reset the device by disconnecting and reconnecting the device to the RP-C room bus. Więcej informacji zawiera Configuring the Room Bus Address for an RP Controller Expansion Sensor Module .Więcej informacji zawiera Connecting RP Controller Expansion Modules to an RP Controller .

Green, flashing fast (~5 Hz)

Device is initializing.

No action required.

Red, flashing (~1 Hz)

Device is non-operational due to a detected error.

Device is forced into maintenance mode.

Contact Schneider Electric Product Support Services for assistance.

Red, flashing fast (~5 Hz)

Device is inoperable due to a detected, non-recoverable error.

Contact Schneider Electric Product Support Services for assistance or return the device to Schneider Electric.

Red, constant

Device is inoperable due to a detected, non-recoverable error.

Return the device to Schneider Electric.

Off mode

The sensor module Status LED is disabled.

  • RP Controller Expansion Modules
  • RP-C-EXT-MS-BLE
  • RP-C-EXT-IS-BLE
  • Configuring the Room Bus Address for an RP Controller Expansion Sensor Module
  • Connecting RP Controller Expansion Modules to an RP Controller
  • Configuring RP Controller Expansion Modules
  • RP Controller Expansion Module Diagnostics
  • RP Controller Expansion Module Maintenance Modes
  • RP Controller Expansion Sensor Module Set Button
  • RP Controller Expansion Module LEDs
  • Status LEDs
  • RP-C Models