earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Pojęcie

Pojęcie


Produkty: RP-C, RP-C-EXT-IS-BLE, RP-C-EXT-MS-BLE
Funkcje: Sprzęt
Wersja produktu: 2022, 2023, 2024, 7.0
2022-04-05

Luminosity Measurement

The RP controller expansion sensor modules support luminosity measurements through an ambient light sensor.

 
action_zoom_plus_stroke Ambient light sensor
Rysunek: Ambient light sensor

The ambient light sensor measures the intensity of visible light. The spectral response of the sensor matches the response of the human eye.

The luminosity range and field of view of the sensor module are specified below.

Luminosity range
Field of view
0 to 10,000 lux
30 degrees from vertical

It is recommended to install the sensor module at least 1 m (3.3 ft) from all windows to help prevent strong sunlight from disturbing the ambient light sensor's luminosity measurements.

 
action_zoom_plus_stroke Luminosity measurement
Rysunek: Luminosity measurement

The luminosity measurements need to be calibrated on site during commissioning. The calibration is done by measuring the light levels in the room using a light meter and then entering a constant lighting reference value (lux) in the EcoStruxure Building Operation software. Więcej informacji zawiera Configuring the RP Controller Expansion Ambient Light Sensor .

  • RP Controller Expansion Modules
  • Sensor Modules
  • RP-C-EXT-MS-BLE
  • RP-C-EXT-IS-BLE
  • Configuring the RP Controller Expansion Ambient Light Sensor