earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Pojęcie

Pojęcie


Produkty: RP-C-EXT-IS-BLE
Funkcje: Sprzęt
Wersja produktu: 2022, 2023
2022-04-05

RP-C-EXT-IS-BLE

The RP-C-EXT-IS-BLE Insight-Sensor connects to the RP controllers and is used for people counting, infrared motion detection, and luminosity and sound pressure level measurements, and supports Bluetooth Low Energy based applications such as beaconing and remote control communication.

The Insight-Sensor provides real-time occupant information that enables immediate control of HVAC for optimized energy consumption and indoor environment, for example, by adapting the fan speed to occupancy level or turning off the lights when unoccupied.

The Insight-Sensor is connected to the RP controller using an RJ45 type quick connector.

The Insight-Sensor's three flexible mounting brackets (springs) enable quick and easy installation on a suspended ceiling tile. The Insight-Sensor also comes with a mounting ring, which allows the device to be installed in open ceiling applications.

The Insight-Sensor is a Bluetooth Low Energy (BLE) device. The Insight-Sensor support for Bluetooth beacon enables nearby mobile devices with a specific app installed to interact when in close proximity to the broadcasting Insight-Sensor. The Bluetooth beacon can be used for services such as indoor positioning of the mobile device. The service and mobile app need to be provided by a third party. The Bluetooth connection can also be used for communication with the RP-C-RC-BLE remote control, which makes it possible to control the lighting, blinds, and air conditioning in a zone of an office building.

The Insight-Sensor is part of the RP controller expansion modules product range. The Insight-Sensor can be combined with the RP controller expansion modules for lighting and blind control to provide a connected room solution.

 
action_zoom_plus_stroke RP-C-EXT-IS-BLE
Rysunek: RP-C-EXT-IS-BLE

People Counting

The Insight-Sensor supports people counting through a thermal image sensor.

Więcej informacji zawiera People Counting .

Motion Detection

The RP controller expansion sensor modules support motion detection through a passive infrared sensor.

Więcej informacji zawiera Motion Detection .

Luminosity Measurement

The RP controller expansion sensor modules support luminosity measurements through an ambient light sensor.

Więcej informacji zawiera Luminosity Measurement .

Sound Pressure Level Measurement

The Insight-Sensor supports sound pressure level measurements through a microelectromechanical system (MEMS) acoustic sensor.

Więcej informacji zawiera Sound Pressure Level Measurement .

Temperature and Humidity Measurement

The Insight-Sensor supports temperature and humidity measurements through a single integrated circuit, consisting of a bandgap temperature sensor and a capacitive humidity sensor.

Więcej informacji zawiera Temperature and Humidity Measurement .

RP Controller Expansion Module Memory

RP controller expansion modules have two types of memory, flash memory and RAM.

Więcej informacji zawiera RP Controller Expansion Module Memory .

RP Controller Expansion Sensor Module Wireless Connectivity

The RP controller expansion sensor modules, such as the Multi-sensor and Insight-Sensor, are Bluetooth Low Energy (BLE) devices, which support applications such as beaconing and remote control communication.

Więcej informacji zawiera RP Controller Expansion Sensor Module Wireless Connectivity .

RP Controller Expansion Module Communication Ports

The RP controller expansion modules have two room bus ports (RJ45 receptacles), which enable connection to the RP-C controller and other expansion modules on the room bus through a daisy-chain configuration.

Więcej informacji zawiera RP-C Room Bus .

RP Controller Expansion Module Address Switch

Each RP controller expansion module has a rotary switch, which is used to give the device a unique address on the room bus.

Więcej informacji zawiera RP-C Room Bus .

RP-C Room Bus

The RP controller room bus allows RP controller expansion modules to be connected to the controller for people counting, motion detection, luminosity and sound pressure level measurements, Bluetooth Low Energy based applications, and control of electric lights and window blinds.

Więcej informacji zawiera RP-C Room Bus .

RP Controller Expansion Sensor Module LED

There is one LED on the RP controller expansion sensor modules. The LED is integrated with the Set button.

Więcej informacji zawiera RP Controller Expansion Sensor Module LED .

RP Controller Expansion Sensor Module Set Button 

The RP controller expansion sensor modules have a Set button on the front. The Set button is reserved for future use.

Więcej informacji zawiera RP Controller Expansion Sensor Module Set Button .

RP Controller Expansion Insight-Sensor Device Installation

The RP controller expansion Insight-Sensor can be installed on a dropped (suspended) ceiling, a drywall ceiling, or a junction (gang) box.

Więcej informacji zawiera RP Controller Expansion Insight-Sensor Device Installation .

Wiring

The wiring recommendations provide guidance regarding wiring of the Central IO modules, automation servers, BACnet/IP devices, RP controller expansion modules, and Operator Display.

Więcej informacji zawiera Wiring .

RP Controller Expansion Module Maintenance Modes

The RP controller expansion modules support different modes that can be used for maintenance purposes.

Więcej informacji zawiera RP Controller Expansion Module Maintenance Modes .

BACnet/IP Device Firmware Management

Using WorkStation, you can update the firmware of multiple BACnet/IP devices and their attached SpaceLogic Sensor devices and RP controller expansion modules at the same time with minimum downtime. In particular, the universal upgrade package simplifies the update process and requires minimal user involvement and coordination.

Uwaga

SpaceLogic Sensor devices and RP controller expansion modules are supported by the RP controller.

Więcej informacji zawiera BACnet/IP Device Firmware Management .

RP Controller Expansion Insight-Sensor Regulatory Compliance and Approvals

This section provides information on regulatory compliance and approvals for the RP controller expansion sensor modules of the Insight-Sensor model.

Więcej informacji zawiera RP Controller Expansion Insight-Sensor Regulatory Compliance and Approvals .

Dane techniczne

Electrical
DC input supply voltage
24 VDC
  
Powered by the RP controller through the room bus (RJ45)
Maximum power consumption
0.35 W
Environment
Ambient temperature, operating
0 to 50 °C (32 to 122 °F)
Ambient temperature, storage
-20 to +70 °C (-4 to +158 °F)
Humidity
20 to 90 % RH non-condensing
Material
Plastic flame rating
UL94 V-0
Ingress protection rating
IP 20
Cover color
Signal white (RAL9003)
Mechanical
 
action_zoom_plus_stroke
Overall external diameter
97.5 mm (3.84 in.)
Diameter of mounting clearance hole
75.0 to 76.0 mm (2.95 to 3.00 in.)
External washer thickness
12 mm (0.47 in.)
Overall external thickness
19 mm (0.75 in.)
Internal thickness
20 mm (0.79 in.)
Overall internal depth
28 mm (1.10 in.)
Weight, Insight-Sensor with mounting springs (3x)
0.088 kg (0.194 lb)
Weight, Insight-Sensor with mounting ring
0.098 kg (0.216 lb)
Installation
Plastic unit to be fitted flush in a suspended ceiling tile with a thickness of up to 45 mm (1.77 in.)
The mounting springs enable quick and easy installation in a suspended celing. The mounting ring allows the device to be installed in a ceiling with drywall anchors or to a 102 mm (4 in.) junction box.
Communication ports
Room bus
RS-485
  
Dual RJ45 ports for daisy-chain configurations
  
Use a Cat 5 (or higher) cable
  
Maximum total length of the room bus: 72 m (236 ft)
Room bus protection
Transient voltage suppressors on communication and power signals
Wireless connectivity
Bluetooth Low Energy
Communication protocol
Bluetooth ® 5.1 Low Energy compliant
Frequency
2.402 to 2.480 GHz
Maximum communication distance
Line-of-sight: 50 m (164 ft)
Maximum output power
3 dBm
Antenna
Integrated antenna
Beacon protocol
iBeacon
Hardware
Main microcontroller
CPU type
ARM Cortex-M4 single-core
Frequency
38.4 MHz
SRAM (embedded)
256 KB
Flash memory (embedded)
1024 KB
Flash memory (serial)
16 MB
Sub microcontroller
CPU type
ARM Cortex-M4 single-core
Frequency
80 MHz
SRAM (embedded)
320 KB
Flash memory (embedded)
1 MB
Flash memory (serial)
2 MB
Additional hardware
Status indicator
LED (green and red) that shows the status of the device
Address switch
Rotary switch 0 to 9
Set button
Push-button switch
People counting
Sensor
Longwave infrared (LWIR) microbolometer
Detection range
See image and table below.
 
action_zoom_plus_stroke

Sensor mounting height

Sensor detection range (diameter) a

3.0 m (10 ft)

7.0 m (22 ft)

2.7 m (9 ft)

5.8 m (19 ft)

2.5 m (8 ft)

5.2 m (17 ft)

Average counting accuracy a
Up to 90%
Motion detection
Sensor
Quad-type passive infrared (PIR) sensor with Fresnel lens
Detection range
See image and table below.
 
action_zoom_plus_stroke

Sensor mounting height

Sensor detection range (diameter)

3.0 m (10 ft)

8.6 m (28 ft)

2.7 m (9 ft)

8.0 m (26 ft)

2.5 m (8 ft)

7.4 m (24 ft)

Luminosity measurements
Sensor
Ambient Light Sensor (ALS)
 
action_zoom_plus_stroke
Spectral response
Human eye
Luminosity range
0 to 10,000 lux
Field of view
30 degrees from vertical
Sound pressure level measurements
Sensor
Microelectromechanical system (MEMS) acoustic sensor
Dynamic pressure
35 to 79 dBA
Accuracy
+/- 3 dBA
Bandwidth
10 Hz to 8 kHz
Temperature measurements
Range
0 to 50 °C (32 to 122 °F)
Accuracy
+/-1 °C (+/-1.8 °F)
Humidity measurements
Range
0 to 100% RH
Accuracy
+/-4% (within the range of 20 to 80% RH)
  
+/-6% (outside the range of 20 to 80% RH)

Internal Configuration

The RP-C-EXT-IS-BLE internal configuration with regards to the signal ground is shown in the following figure.

 
action_zoom_plus_stroke RP-C-EXT-IS-BLE internal configuration
Rysunek: RP-C-EXT-IS-BLE internal configuration
  • Hardware Overview
  • RP Controller Expansion Modules
  • Sensor Modules
  • People Counting
  • Motion Detection
  • Luminosity Measurement
  • Sound Pressure Level Measurement
  • Temperature and Humidity Measurement
  • RP Controller Expansion Module Memory
  • RP Controller Expansion Sensor Module Wireless Connectivity
  • RP-C Room Bus
  • RP Controller Expansion Sensor Module LED
  • RP Controller Expansion Sensor Module Set Button
  • RP Controller Expansion Insight-Sensor Device Installation
  • Wiring
  • RP Controller Expansion Module Maintenance Modes
  • BACnet/IP Device Firmware Management
  • RP Controller Expansion Insight-Sensor Regulatory Compliance and Approvals