The RP controller expansion sensor modules can be used, for example, for infrared motion detection and luminosity measurement.
The sensor modules are available in different models with different sets of sensors that provide support for various sensor features.
Module |
People Counting |
Motion Detection |
Luminosity Measurement |
Sound Pressure Level Measurement |
Temperature and Humidity Measurement |
RP-C-EXT-IS-BLE |
yes |
yes |
yes |
yes |
yes |
RP-C-EXT-MS-BLE |
no |
yes |
yes |
no |
no |
The RP-C-EXT-IS-BLE Insight-Sensor connects to the RP controllers and is used for people counting, infrared motion detection, and luminosity and sound pressure level measurements, and supports Bluetooth Low Energy based applications such as beaconing and remote control communication.
Więcej informacji zawiera RP-C-EXT-IS-BLE .
The RP-C-EXT-MS-BLE multi-sensor connects to the RP-C room controllers and is used for infrared motion detection and luminosity measurements. The multi-sensor supports Bluetooth Low Energy based applications such as beaconing and remote control communication.
Więcej informacji zawiera RP-C-EXT-MS-BLE .