The RP Series expansion modules have PCB mounted connectors for the power input, outputs and digital inputs. The connectors are mechanically keyed and color-coded, which allows the matching external connectors to be plugged in on site quickly and easily.
The pluggable connectors mean time savings and cost reductions for the installation, compared to wiring terminal blocks on site. The connectors can quickly and easily be plugged together on site.
The RP Series expansion modules use 2, 3, 4 or 5 pole connectors for the different inputs and outputs. The 4-pole connector has a 5-pole frame.
The connectors are mechanically keyed, which means the following connections cannot be made:
A connector for AC mains and high-voltage applications cannot be plugged into a connector for low-voltage applications.
A connector for low-voltage applications cannot be plugged into a connector for AC mains and high-voltage applications.
The matching connectors are locked together.
The connectors are also color-coded to help the installers and electricians to choose the correct, matching external connector. The connectors are color-coded:
Black: For AC mains power applications such as power supply input, blind high-voltage outputs, SMI (HV) blind outputs, and relay outputs.
Pastel blue: For dimming applications such as DALI light outputs and 0-10V light outputs with power distribution.
Light blue: For low-voltage applications such as blind low-voltage outputs (24 VDC), 0-10V light outputs without power distribution, SMI LoVo (LV) blind outputs, and digital inputs (5 VDC).
The matching external connectors are not provided but need to be ordered separately from Schneider Electric. For more information, see Required External Connectors for the RP Series Expansion Modules .