Use the device detail screen to interact with the device and its features.
The device detail screen is also available with configuration menus. For more information, see Device Detail Screen (with Configuration Menus) .
Component |
Description |
Alarms |
Tap to open the Alarms screen, where you view and acknowledge alarms specific to this device. This option is only visible if alarms are configured on this device. For more information, see Alarms Screen . |
Inputs |
Tap to open the Inputs screen, where you view and edit the analog, binary, and multi-state inputs. This option is only visible if inputs are configured on this device. For more information, see Inputs Screen . |
Outputs |
Tap to open the Outputs screen, where you view and edit the analog, binary, and multi-state outputs. This option is only visible if outputs are configured on this device. For more information, see Outputs Screen . |
Values |
Tap to open the Values screen, where you view and edit the analog, binary, and multi-state values. This option is only visible if values are configured on this device. For more information, see Values Screen . |
Schedules |
Tap to open the Schedules screen, where you view and edit schedule events specific to this device. This option is only visible if schedules are configured on this device. For more information, see Schedules Screen . |
Trend Logs |
Tap to open the Trend Logs screen, where you view event logs specific to this device. This option is only visible if trend logs are configured on this device. For more information, see Trend Logs Screen . |
Device Info |
Tap to open the Device Info screen, where you view more information on the device and rediscover to refresh its inputs, outputs, and values. For more information, see Device Info Screen . |