earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: Sustainability
产品版本: 2024, 7.0
2024/12/10

Meter Processor – Outputs Tab

Use the Meter Processor – Outputs tab to view the output from the meter processor.

 
action_zoom_plus_stroke Meter Processor – Outputs tab
图: Meter Processor – Outputs tab

表格: Meter Processor – Outputs Tab

Component

Description

Meter value (kWh)

Displays the total meter processor value output. Read-only.

Suppressed reduction (kWh)

Displays the suppressed reduction that avoids negative consumptions. 有关更多信息,请参阅 Meter Processor Suppressed Reduction .

Current hour (kWh)

Displays the consumption during the current hour. Read-only.

Current day (kWh)

Displays the consumption during the current day. Read-only.

Current week (kWh)

Displays the consumption during the current week. Read-only.

Current month (kWh)

Displays the consumption during the current month. Read-only.

Current year (kWh)

Displays the consumption during the current year. Read-only.

  • Energy Consumption Overview
  • Meter Processor Suppressed Reduction
  • Consumption Signature – Expected Consumption Signature Curve Tab
  • Consumption Signature - Basic Tab
  • Consumption Signature – Output Consumption Tab
  • Consumption Signature – Input Consumption Tab
  • Meter Processor – Basic Tab
  • Meter Object – Outputs Tab
  • Meter Object – Basic Tab