earth_america
user_standard Iniciar sessão
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interface de utilizador

Interface de utilizador


Produtos: AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Alarmes
Versão do produto: 3.2, 3.3, 2022
30-04-2021

Attachment Properties

Use the Attachment properties to edit attachments and configure whether or not the attachments are displayed when the alarm is triggered.

 
action_zoom_plus_stroke Attachment properties
Imagem: Attachment properties

Tabela: Attachment Properties

Component

Description

Display on alarm

Select True to to automatically open and display the attachment when the alarm is going from Normal to Alarm state.

Object reference

Enter the path to the item you want to attach to the alarm.

  • Anexos de alarme
  • Adding an Attachment to an Alarm
  • Adding an Attachment to Multiple Alarms
  • Removing an Attachment from an Alarm
  • Removing Attachments from Multiple Alarms