earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 时间表
产品版本: 2024, 7.0
2024/12/3

Creating a Digital Schedule

You create a digital schedule to control the state of a digital value.

显示更多
action_close

A digital schedule controls a device that has an on output state and an off output state.

For example, you can create a digital weekly schedule that is bound to a digital output, such as a light switch. To turn on the lights Monday through Friday from 08:00 to 17:00, you can set the value to On when the schedule is active and Off when the schedule is inactive.

 
action_zoom_plus_stroke Digital Schedule
图: Digital Schedule

To create a digital schedule
  1. In WorkStation, in the System Tree pane, select the EcoStruxure BMS server or the folder where you want to create the schedule.

  2. On the File menu, point to New and then click Schedule .

  3. In the Create Object wizard, in the object type list, select Digital Schedule .

  4. In the Name box, type a name for the schedule.

  5. In the Description box, type a description for the schedule.

  6. Click Create .

Now you can add events to the digital schedule and bind it to a digital value.

  • Adding a Weekly Event
  • Create Object Dialog – Naming the Object Page
  • Binding a Digital Value to a Digital Schedule
  • Adding a Calendar Exception Event
  • Adding a Date Exception Event
  • Adding a Date Range Exception Event
  • Adding a Calculated Exception Event
  • Digital Schedules
  • Schedule Types
  • Create Object Dialog – Naming the Object Page