earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, WorkStation, Project Configuration Tool
功能: 时间表
产品版本: 2023
2022/12/17

Creating an Analog Schedule

You create an analog schedule to control the state of an analog value.

显示更多
action_close

An analog schedule controls a device that gauges the output in real numbers. The real numbers include positive or negative numbers, fractions, and decimal values.

例如,您可以创建模拟时间表以在办公区中控制恒温设定值。要控制 08:00 到 17:00 的温度,可将值设置为当时间表激活时为“22 °C (72 °F)”,当时间表未激活时为“16 °C (62 °F)”。

 
action_zoom_plus_stroke 模拟时间表
图: 模拟时间表

To create an analog schedule
  1. In WorkStation, in the System Tree pane, select the EcoStruxure BMS server or the folder.

  2. On the File menu, point to New and then click Schedule .

  3. In the Create Object wizard, in the object type list, select Analog Schedule .

  4. In the Name box, type a name for the schedule.

  5. In the Description box, type a description for the schedule.

  6. Click Create .

Now you can add events to the analog schedule and bind the schedule to an analog value.

  • 时间表类型
  • 模拟时间表
  • Binding an Analog Value to an Analog Schedule
  • 添加每周事件
  • 添加日历例外事件
  • 添加日期例外事件
  • 添加日期范围例外事件
  • 添加计算的例外事件
  • Create Object Dialog – Naming the Object Page