earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, WorkStation, Project Configuration Tool
功能: 时间表
产品版本: 2024, 7.0
2024/12/3

Creating an Analog Schedule

You create an analog schedule to control the state of an analog value.

显示更多
action_close

An analog schedule controls a device that gauges the output in real numbers. The real numbers include positive or negative numbers, fractions, and decimal values.

For example, you can create an analog schedule to regulate a thermostat setpoint in an office area. To control the temperature from 08:00 to 17:00, you can set the value to 22 °C (72 °F) when the schedule is active and 16 °C (62 °F) when the schedule is inactive.

 
action_zoom_plus_stroke Analog Schedule
图: Analog Schedule

To create an analog schedule
  1. In WorkStation, in the System Tree pane, select the EcoStruxure BMS server or the folder.

  2. On the File menu, point to New and then click Schedule .

  3. In the Create Object wizard, in the object type list, select Analog Schedule .

  4. In the Name box, type a name for the schedule.

  5. In the Description box, type a description for the schedule.

  6. Click Create .

Now you can add events to the analog schedule and bind the schedule to an analog value.

  • Schedule Types
  • Analog Schedules
  • Binding an Analog Value to an Analog Schedule
  • Adding a Weekly Event
  • Adding a Calendar Exception Event
  • Adding a Date Exception Event
  • Adding a Date Range Exception Event
  • Adding a Calculated Exception Event
  • Create Object Dialog – Naming the Object Page