earth_america
user_standard Accedi
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concetto

Concetto


Prodotti: AS-B, Enterprise Central, Enterprise Server, AS-P, WorkStation, Project Configuration Tool
Funzionalità: Funzionalità di base
Versione del prodotto: 3.2, 3.3, 2022
15/10/2020

Log on to WorkStation or WebStation

arrow1_rotationLog on to WorkStation arrow1_rotationLog on to WebStation

You log on to WorkStation or WebStation to securely access the EcoStruxure Building Operation functions.

Log on to WorkStation

You log on to WorkStation with your current Windows credentials, as another Windows user, or as an EcoStruxure Building Operation user. Your system administrator decides which type of user you log on as. ​

To log on to WorkStation using an EcoStruxure Building Operation account, you need to know the following account information:

  • User name

  • Password

  • Domain

  • EcoStruxure BMS server

To log on to WorkStation using a Windows account, you need to know the EcoStruxure BMS server.

The account information for both the EcoStruxure Building Operation account and the Windows account is provided by the system administrator.

Avviso

​​Ensure that you have a working and available WorkStation license. A working license is required to log on to WorkStation. Per maggior informazioni, consulta EcoStruxure Building Operation Software Licensing Installation and Location .

Remember me on this computer

For a faster log on in Workstation, use the Remember me feature to automatically fill in your user name, password, domain and server. Both Building Operation users and Windows users can use the Remember me feature.

Add a display name of the server address

When you log on to a new server, its IP address is added to the server list. You can add a display name of the server address to make it easier to find your server in the list.

Log on to WebStation

To log on to WebStation, you need to know the following account information:

  • User name

  • Password

  • Domain

  • EcoStruxure BMS server

The account information for your account is provided by the system administrator.

  • Panoramica di WorkStation
  • Panoramica di WebStation
  • Accesso a WorkStation utilizzando il proprio account utente di Windows
  • Accesso a WorkStation come altro utente Windows
  • Accesso a WorkStation come utente di EcoStruxure Building Operation
  • Disconnessione da WorkStation
  • Accesso a WebStation
  • Disconnessione da WebStation
  • Salvataggio delle informazioni di accesso
  • Changing Your Password
  • Modifica della password
  • Aree di lavoro
  • Selezione di un'area di lavoro predefinita
  • Cambio di aree di lavoro
  • Building Operation WorkStation Window
  • Finestra Building Operation in WebStation
  • Change Password Dialog Box