Funzionalità: Tendenza
Versione del prodotto: 2023
17/12/2022

Manual Trend Logs

​The manual trend log records data that you manually enter. The manual trend log does not log a variable. Use this type of trend log when values from offline devices have to be manually registered to the trend log. For example, if you want to create a trend log that monitors an electricity meter that cannot be connected to the EcoStruxure BMS.

The default size of a manual trend log is 100 records.

 
action_zoom_plus_stroke Manual trend log schematic.
Figura: Manual trend log schematic.
Manual trend log meter functionality

A manual trend log can be created with initial meter settings. The manual trend log supports the meter change command and meter consumption calculation. You can view the last meter change information on the manual trend log object. Per maggior informazioni, consulta Funzione Contatore .

  • Trend Log Types
  • Creating a Manual Trend Log
  • Configuring a Manual Trend Log
  • Trend Units
  • Memoria di registrazione
  • Funzione Contatore
  • Manual Trend Log Properties – Basic Tab
  • Manual Trend Log Properties – Meter Info Tab
  • References Tab
  • Trend Log estesi