earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Explicación de procesos

Explicación de procesos


Productos AD v2, AD v1, Technician Tool for Android, Technician Tool for iOS
Funcionalidades: Funcionalidad básica
Versión del producto: 1.8, 1.9
09/02/2018
Haga clic para ver la versión actualizada que aún no se ha traducido

Cómo añadir un servidor SmartStruxure a Favoritos

Puede añadir un servidor SmartStruxure a Favoritos para que pueda conectarse rápidamente a él.

Mostrar más
action_close

Technician Tool is used to access the functions in Building Operation. You use Technician Tool to view and monitor all work on a daily basis in Building Operation. You can change the value for an event to control the output state of a device. You can also force a value when you want to override a value, such as a value from a device.

Log On

You log on to Technician Tool to securely access the functions in Building Operation. You can log on directly from Favorites if the SmartStruxure server is added or by typing log on credentials.

Para obtener más información, consulte Inicio de sesión en Technician Tool .

Para obtener más información, consulte Cómo iniciar sesión en Technician Tool desde Favoritos .

User Account Profile Workflow

User accounts are used to control user activities in Technician Tool.

For example, in Workstation, you create a Custom View that contains variables of a Campus that you want to monitor from Technician Tool. The Campus has four buildings: Administration, East, South, and Northwest.

You then create the user profiles that have access to a specific part of the building:

  • A team dedicated to East aisle, having access to all information of Building - East

  • A team dedicated to South aisle, having access to energy values in Read/Write and HVAC value in Read only mode of Building - South

  • A team dedicated to the entire Building

Para obtener más información, consulte Flujo de trabajo del perfil de la cuenta de usuario .

Favorites

You can add SmartStruxure servers and folders to Favorites, so you can quickly access them. When you add a SmartStruxure server in Favorites, you can log on directly without typing the SmartStruxure server IP address, name, and password. You can group SmartStruxure servers in the folders added in Favorites.

Para obtener más información, consulte Cómo añadir un servidor SmartStruxure a Favoritos .

Para obtener más información, consulte Cómo añadir una carpeta a Favoritos .

Views

In Technician Tool, you can display the Building Operation database in two ways:

  • Custom view: Displays only the objects and folders that you want to see in the order that you want.

  • System view: Displays the entire tree structure of Building Operation as it appears in WorkStation.

Para obtener más información, consulte Vista personalizada .

Para obtener más información, consulte Sistema .

Alarms

You are notified by alarms when an important event occurs. For example, if the temperature is too low or too high in a building, if a window is open, or if something is broken, such as a fan. The system administrator sets up the alarms and decides to whom the alarm is sent.

Para obtener más información, consulte Alarmas .

Localization

By default, iphone presents language, date, time, currency, unit, and decimals according to the regional settings of your iphone.

Technician Tool supports several different languages (English, French, Swedish, German, Finnish, and Spanish). You can change the language of your iphone to view the Technician Tool user interface in a different language.

After you change the language, you need to restart the Technician Tool and log on again for the changes to take effect.

Search

Use Search to filter out the objects and variables in Custom View and System so that you do not have to browse through the long list of variables to locate the ones that concern you. Searches are folder based. You can search for the objects and variables within a particular folder.

Para obtener más información, consulte Buscar .

Technician Tool and WebStation Differences

There are a number of differences in functionality between Technician Tool and WebStation.

Para obtener más información, consulte Technician Tool and WebStation Differences .

Para añadir un servidor SmartStruxure a Favoritos
  1. En Technician Tool, pulse en Favoritos .

  2. Pulse Añadir para iOS o toque

     
    action_zoom_plus_stroke
    para Android.

     
    action_zoom_plus_stroke
  3. Pulse Servidor en los dispositivos iOS o toque el tipo de servidor de SmartStruxure en el que desea iniciar sesión en los dispositivos de Android.

     
    action_zoom_plus_stroke
  4. En el cuadro Nombre introduzca el nombre con el que el servidor SmartStruxure se mostrará en Favoritos.

     
    action_zoom_plus_stroke

  5. En el cuadro Descripción introduzca una descripción para el servidor SmartStruxure.

  6. En el cuadro Servidor introduzca un nombre de servidor SmartStruxure o una dirección IP.

  7. En el cuadro Nombre de usuario , introduzca un nombre de usuario.

  8. En el cuadro Contraseña , introduzca una contraseña.

     
    action_zoom_plus_stroke

  9. en los dispositivos iOS toque el tipo de servidor de SmartStruxure en el que desea iniciar sesión.

  10. Pulse Hecho para iOS o toque

     
    action_zoom_plus_stroke
    para Android.

  11. Pulse Hecho en los dispositivos iOS.

  • Technician Tool Overview
  • Cómo añadir una carpeta a Favoritos