earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Enterprise Central, Enterprise Server, FDP Server
Functionalities: Sustainability
12/10/2024

Consumption Signature – Output Consumption Tab

Use the Consumption Signature – Output consumption tab to view the consumption during a specific time period.

 
action_zoom_plus_stroke Consumption Signature – Output consumption tab
Figure: Consumption Signature – Output consumption tab

Table: Consumption Signature – Output Consumption Tab

Component

Description

Enable output consumption

Actual consumption

Displays the actual consumption, that is the calculated consumption from the consumption log.

Expected consumption

Displays the expected consumption, that is the expected consumption according to the signature curve.

Consumption difference

Displays the consumption difference if the consumption is higher or lower than the expected consumption.

Dependency value

Displays the dependency value, that is the calculated dependency value from the dependency log.

Period start

Period end

  • Energy Consumption Overview
  • General Information Properties – Basic Tab
  • Consumption Signature – Output Consumption Tab