earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Operator Display
Functionalities: Basic Functionality, BACnet/IP devices, Localization, Upgrade, User Management
Product version: 3.3, 2022, 2023, 2024, 7.0, 7.1
1/25/2023

Operator Display Settings Screen

Use the Operator Display Settings screen to configure Operator Display and perform administrative tasks.

 
action_zoom_plus_stroke Operator Display Settings screen
Figure: Operator Display Settings screen

Table: Operator Display Settings Screen

Component

Description

Language

Tap to open the Language settings screen where you select a language for menus and options. For more information, see Language Setting Screen .

This task requires administrator permissions.

Units

Tap to open the Units screen where you can select the temperature setting. For more information, see Units Screen .

Time

Tap to open the Date / Time screen where you set the time and date. For more information, see Date / Time Screen .

Network

Tap to open the Network Setup screen where configure the IP network communication. For more information, see Network Setup Screen .

BACnet

Tap to open the BACnet Setup screen where you configure the BACnet/IP network communication. For more information, see BACnet Setup Screen .

Firmware Upgrade

Tap to open the Firmware Update screen where you upload a new version of the Operator display firmware. For more information, see Firmware Update Screen .

This task requires administrator permissions.

Display

Tap to open the Display screen where you configure the backlight setttings. For more information, see Display Screen .

This task requires administrator permissions.

User Configuration

Tap to open the User Configuration screen where you configure the setttings for all users. For more information, see User Configuration Screen .

This task requires administrator permissions.

User Administration

Tap to open the User Administration screen where you create and delete users. For more information, see User Administration Screen .

This task requires administrator permissions.

About

Tap to open the About screen where you view more information on Operator Display. For more information, see About Screen .

  • Language Setting Screen
  • Units Screen
  • Date / Time Screen
  • Network Setup Screen
  • BACnet Setup Screen
  • Firmware Update Screen
  • Display Screen
  • User Configuration Screen
  • User Administration Screen
  • About Screen