earth_america
user_standard Log on
action_search_stroke
earth_america

BACnet/IP Devices

RP-C
RP-V
MP-C
MP-V
IP-IO
RP-IO
MP-C Smoke Control
MP-V Smoke Control
IP-IO Smoke Control
Refine your search
arrow2_down
Refine your search
Ok
Ok
Ok

211 Topic(s)

Concept

The wiring recommendations provide guidance regarding wiring of the I/O modules, SmartX servers, and MP Series controllers.

User Interface

The Status LED on the front of the SmartX devices changes color and flashes to indicate the status of the device.

Concept

The I/O wiring recommendations provide guidance on what type of wires should be used for the different I/O modules, SmartX AS-B server onboard I/O, and MP Series controller onboard I/O, how to perform grounding, and how to connect different external devices to the inputs and outputs. Always use the recommended cables and wires.

Concept

The Schneider Electric hardware devices for the EcoStruxure BMS include terminal bases, PS-24V power supplies, SmartX servers such as SmartX AS-P servers and SmartX AS-B servers, MP Series controllers such as MP-Cs and MP-Vs, I/O modules, and ADs.

Concept

It is important to perform the grounding correctly for the following reasons:

Concept

There are many different kinds of external devices from different vendors that can be connected to an EcoStruxure BMS.

Specifications

How to

You wire the terminal blocks installed on the IP-IO module to connect I/O devices and power.

How to

You remove a terminal block from an IP-IO module in order to replace the module.

Hardware Installation

Part number: SXWMPCDSP10A01