earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Automation Server, AS-B, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: User Management
Product version: 1.9
12/14/2016

Removing Path Permissions from a User Account

You remove a permission of an individual user account to a folder or an object when the user account no longer is to access the folder or object.

Show More
action_close

​Path permissions are used to give a user account group or a user account access to the objects defined in the path. The permissions configured on a path apply to all path sub-levels unless you configure new permissions for the path sub-level.

For more information, see Software Permission Rules .

Example

A user has the full set of permissions: Read, Write, Create, Delete, Edit, and Force to the folder Building A. The user account group also has Read permissions to the folder Building B, but No access to the sub-folders of Building B. Therefore, the user has permission to navigate and modify the objects in the Building A folder, but only permission to view the objects in the Building B main folder.

 
action_zoom_plus_stroke Path permissions in Building Operation
Figure: Path permissions in Building Operation

Path Permissions Example

A user account group has the full set of path permissions to the Enterprise Server and no permissions to the Servers folder on the Enterprise Server. A single user account has the full set of path permissions to Automation Server 1, but no path permission to Automation Servers 2 and 3. Even though the user account group has no path permission to the Servers folder, it is possible to give individual user accounts access to individual Automation Servers in the Servers folder.

For more information, see Path Permissions Example .

Context-Sensitive Path Permissions

You can manage permissions by configuring the permissions for a given user account or user account group to a certain object in the System Tree pane or List View and below that object, for example, a folder and its contents.

For more information, see Context-Sensitive Path Permissions .

To remove path permissions from a user account
  1. In WorkStation, on the Tools menu, click Control Panel .

  2. On the Control Panel toolbar, select the SmartStruxure server.

     
    action_zoom_plus_stroke
  3. Click Account management .

  4. In the Domain list, select the domain the user account belongs to.

     
    action_zoom_plus_stroke
  5. In the User Accounts list, select the user account whose path permissions you want to remove.

  6. Click Software Permissions .

  7. In the Path list, select the path whose permissions you want to remove from the user account.

     
    action_zoom_plus_stroke
  8. Click the Remove button

     
    action_zoom_plus_stroke
    .

  • Path Permissions
  • Software Permissions
  • Assigning Path Permissions to a User Account
  • Editing the Path Permissions of a User Account
  • User Account – Software Permissions Tab
  • Removing Path Permissions from a User Account
  • Account Management Control Panel
  • Software Permission Rules