earth_america
user_standard Accedi
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Modalità

Modalità


Prodotti: AS-C, AS-B, Enterprise Server, AS-P, Project Configuration Server, Project Configuration Tool
Funzionalità: Gestione dell'utente
Versione del prodotto: 1.8
14/03/2018

Removing Software Permissions from a User Account

You remove a user account's individual path permission to remove the permission to a folder or an object the user account no longer is to have permissions to.

Mostra di più
action_close

​Path permissions give a user or user account group basic permissions to the objects defined in a path. The permission level set on a path applies to all sub levels unless you set a new permission level for a sub level.

The following permissions can be set for a path:

  • No Access: Users cannot navigate to or modify any of the objects in the path.

  • Read: Users can navigate to the objects but cannot modify them.

  • Full Access: Users can navigate to and modify the objects.

Example

A user has the permission Full Access to the folder Building A. The user account group also has Read permissions to the folder Building B, but No access to the subfolders of Building B. Therefore the user has permission to navigate and modify the objects in the Building A folder, but only permission to view the objects in the Building B main folder.

 
action_zoom_plus_stroke Path permission levels in Building Operation
Figura: Path permission levels in Building Operation

Path Permissions Example

A user account group has the permission Full Access to the Enterprise Server and No Access to the Servers folder on the Enterprise Server. A single user account has Full Access permissions to Automation Server 1, but No Access to Automation Servers 2 and 3. The No Access permission on the Servers folders makes it possible to give specific user accounts access to specific Automation Servers in that folder.

Per maggior informazioni, consulta Path Permissions Example .

Context-Sensitive Path Permissions

You can manage permissions by configuring the permissions for a given user account or user account group to a certain object in the System Tree pane or List View and below that object, for example, a folder and its contents.

Per maggior informazioni, consulta Context-Sensitive Path Permissions .

To remove software permissions from a user account
  1. In WorkStation, on the Tools menu, click Control Panel .

  2. On the Control Panel toolbar, select the SmartStruxure server.

     
    action_zoom_plus_stroke
  3. Click Account management .

  4. In the Domain list, select the domain the user account belongs to.

     
    action_zoom_plus_stroke
  5. In the User Accounts list, select the user account whose path permissions you want to remove.

  6. Click Software Permissions .

  7. In the Path list, select the path whose permissions you want to remove from the user account.

     
    action_zoom_plus_stroke
  8. Click the Remove button

     
    action_zoom_plus_stroke
    .

  • Path Permissions
  • Software Permissions
  • Assigning Software Permissions to a User Account
  • Editing the Software Permissions of a User Account
  • User Account – Software Permissions Tab
  • Removing Software Permissions from a User Account
  • Account Management Control Panel
  • Software Permission Rules