earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AS-P Smoke Control, Automation Server Smoke Control, IP-IO Smoke Control, MP-C Smoke Control, MP-V Smoke Control
Functionalities: Smoke Control
Product version: 3.0
10/28/2020

MNA-FLO-1 Enclosure

arrow1_rotationFront View arrow1_rotationInside View arrow1_rotationPhysical Dimensions arrow1_rotationMounting Dimensions

The UL 864 listed MNA-FLO-1 enclosure is a 2.75-inch deep (69.85 mm) box designed for use with VAV controllers.

Front View

The following illustration shows the front view of the enclosure.

 
action_zoom_plus_stroke MNA-FLO-1 Enclosure - Front Panel
Figure: MNA-FLO-1 Enclosure - Front Panel

As shown, the front view includes a product and smoke control label and an enclosure cover.

Inside View

The following illustration shows the inside view of the enclosure.

 
action_zoom_plus_stroke MNA-FLO-1 Enclosure - Inside View
Figure: MNA-FLO-1 Enclosure - Inside View

As shown, the inside of the enclosure includes a b3/i2865-V-S controller, an enclosure base, a damper shaft, a product label, and a mounting tab.

Physical Dimensions

The following illustration shows the physical dimensions of the enclosure.

 
action_zoom_plus_stroke MNA-FLO-1 Enclosure - Front Dimensions
Figure: MNA-FLO-1 Enclosure - Front Dimensions

The MNA-FLO-1 provides knockouts in the positions shown for .50 inches (12.70 mm) or .75 inches (19.05 mm) conduit connections.

Mounting Dimensions

The following illustration shows the mounting dimensions of the enclosure.

 
action_zoom_plus_stroke MNA-FLO-1 Enclosure - Mounting Dimensions
Figure: MNA-FLO-1 Enclosure - Mounting Dimensions
  • Smoke Control Recommended Enclosures
  • SEBOX121806 Enclosure
  • SEBOX161608 Enclosure
  • SEBOX202010 Enclosure
  • SEBOX242408 Enclosure
  • SEBOX392410 Enclosure
  • SEBOX393210 Enclosure
  • UL 864 Smoke Control Enclosure Mounting Hardware
  • Mounting a UL 864 Smoke Control Enclosure