The SEBOX202010 enclosure is a 9.8 inch deep (250 mm), compact, multi-purpose box. Its features include a reversible door with invisible hinges that open 120 degrees, a standard 3mm double bar lock with screw driver lock feature and a foamed-in polyurethane gasket door that prevents water and dust migration. An optional key lock is also available. You can order the enclosures with an optional perforated back plate using the P suffix on the model. The SEBOX202010 is designed for use with EcoStruxure Building Operation components, such as Automation Servers, Power Supplies, MP controllers and Central IO modules.
The SEBOX201010 is a wall-mounted enclosure with the following dimensions:
Height: 19.7 inch (500 mm)
Width: 19.7 inch (500 mm)
Depth: 9.8 inch (250 mm)
Cubic inch volume: 3803 (62500 cu. cm)
For more information, see Mounting a UL 864 Smoke Control Enclosure .