The SEBOX161608 is a 7.9 inch deep (200 mm), compact, multi-purpose box. Its features include a reversible door with invisible hinges that open 120 degrees, a standard 3mm double bar lock with screw driver lock feature and a foamed-in polyurethane gasket door that prevents water and dust migration. An optional key lock is also available. You can order the enclosures with an optional perforated back plate using the P suffix on the model. The SEBOX161608 is designed for use with EcoStruxure Building Operation components, such as Automation Servers, Power Supplies, MP controllers and Central IO modules.
The SEBOX161608 is a wall-mounted enclosure with the following dimensions:
Height: 15.6 inch (400 mm)
Width: 15.6 inch (400 mm)
Depth: 7.9 inch (200 mm)
Cubic inch volume: 1922 (32000 cu. cm)
For more information, see Mounting a UL 864 Smoke Control Enclosure .