The SEBOX242408 enclosure is a 7.9 inch (200 mm) deep compact, multi-purpose box. Its features include a reversible door with invisible hinges that open 120 degrees, a standard 3mm double bar lock with screw driver lock feature and a foamed-in polyurethane gasket door that prevents water and dust migration. An optional key lock is also available. You can order the enclosures with an optional perforated back plate using the P suffix on the model. The SEBOX242408 is designed for use with EcoStruxure Building Operation components, such as Automation Servers, Power Supplies, MP controllers and Central IO modules.
The SEBOX242408 is a wall-mounted enclosure with the following dimensions:
Height: 23.6 inch (600 mm)
Width: 23.6 inch (600 mm)
Depth: 7.9 inch (200 mm)
Cubic inch volume: 4400 (72000 cu. cm)
For more information, see Mounting a UL 864 Smoke Control Enclosure .