Using a WiFi router containing a DHCP server, you can temporarily set up a WiFi network to wirelessly connect the eCommission SmartX Controllers mobile application to the SmartX IP controller network.
Configure the DHCP server on the WiFi router as needed, including a suitable IP address range.
Configure the network settings on the mobile device running the eCommission application to connect to the WiFi router.
On the mobile device, enable WiFi and then connect to the wireless network.
In the eCommission application, on the Select Connection view, select the WiFi icon
In the Device List view, select the SmartX IP controllers to make the connection.
Using the eCommission application, you can now perform tasks on the connected SmartX IP controllers as needed.