Running the eCommission SmartX Controllers mobile application on a Windows laptop computer, you can connect directly to a SmartX IP controller by Ethernet wire. Optionally, you can use an Ethernet switch to connect the computer and the SmartX IP controller.
Configure the network connections on the eCommission application computer and the SmartX IP controller for DHCP addressing.
For more information, see Configuring SmartX IP Controller Device Settings .
Connect an Ethernet cable between the eCommission application computer and Port 1 of the SmartX IP controller. If you are using an Ethernet switch, connect the computer and the controller to the switch, using Ethernet cables.
Because an actual DHCP server is not used, both the eCommission application computer and the SmartX IP controller will self-assign link-local IP addresses.
In the eCommission application, on the Select Connection view, select the WiFi icon
In the Device List view, select the SmartX IP controller to make the connection.
Using the eCommission application, you can now perform tasks on the connected SmartX IP controller as needed.