You can use a wireless access point to connect the eCommission SmartX Controllers mobile application to the SmartX IP controller network.
Confirm that the access point is connected to a wired network containing a DHCP server.
Configure the network settings on the mobile device running the eCommission application to connect to the WiFi network containing the SmartX IP controllers.
On the mobile device, enable WiFi and then connect to the wireless network.
In the eCommission application, on the Select Connection view, select the WiFi icon
In the Device List view, select the SmartX IP controllers to make the connection.
Using the eCommission application, you can now perform tasks on the connected SmartX IP controllers as needed.