Running the eCommission SmartX Controllers mobile application on a Windows laptop computer, you can connect directly to an Ethernet port on a networked BACnet/IP controller, or use an Ethernet switch to connect to a group of controllers.
Configure the network connections on the eCommission application computer and the BACnet/IP controllers:
For more information, see Configuring BACnet/IP Device Settings .
If the network contains a DHCP server, configure these network connections for DHCP addressing.
If the network does not contain a DHCP server, configure these network connections for static IP addressing.
Connect an Ethernet cable between the eCommission application computer and Port 1 of an BACnet/IP controller on the network. If you are using an Ethernet switch, connect the computer and the controllers to the switch, using Ethernet cables.
In the eCommission application, on the Select Connection view, select the WiFi icon
In the Device List view, select the BACnet/IP controllers to make the connections.
Using the eCommission application, you can now perform tasks on the connected BACnet/IP controllers as needed.