earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Commission, IP-IO , MP-C, MP-V, RP-C
Functionalities: Engineering, BACnet/IP devices
Product version: 3.3
7/18/2021

Connecting to Network of BACnet/IP Controllers through a Wireless Access Point

You can use a wireless access point to connect the eCommission SmartX Controllers mobile application to the BACnet/IP controller network.

Show More
action_close

Use this workflow to connect the eCommission SmartX Controllers mobile application to BACnet/IP controllers.

Related information can be found in the sections that follow the flowchart.

 
action_zoom_plus_stroke eCommission Application Connection Workflow
Figure: eCommission Application Connection Workflow
Download, install, and activate the eCommission application

Download, install, and activate the eCommission application, and accept the end user license agreement.

For more information, see Downloading and Starting the eCommission SmartX Controllers Mobile Application .

For more information, see Launching and Activating the eCommission SmartX Controllers Mobile Application .

Power up the controllers

Power up the BACnet/IP controllers.

For more information, see Powering Up MP-C .

For more information, see Powering Up MP-V .

Prepare a wired or wireless connection for eCommission application

Prepare a wired or wireless connection for use with the eCommission application mobile device.

Connection Type

More Information

Wired connection to a single controller

For more information, see Connecting to Single BACnet/IP Controller by Wire .

Wired connection to a network of controllers

For more information, see Connecting to Network of BACnet/IP Controllers by Wire .

Wireless connection to a network of controllers via a WiFi router

For more information, see Connecting to Network of BACnet/IP Controllers through WiFi Router .

Wireless connection to a network of controllers via a wireless access point

For more information, see Connecting to Network of BACnet/IP Controllers through a Wireless Access Point .

Start the eCommission application and discover controllers

Start the eCommission application and then discover the BACnet/IP controllers on the network.

For more information, see Downloading and Starting the eCommission SmartX Controllers Mobile Application .

To connect to a network of BACnet/IP controllers through a wireless access point
  1. Confirm that the access point is connected to a wired network containing a DHCP server.

  2. Configure the network settings on the mobile device running the eCommission application to connect to the WiFi network containing the BACnet/IP controllers.

  3. On the mobile device, enable WiFi and then connect to the wireless network.

  4. In the eCommission application, on the Select Connection view, select the WiFi icon

     
    action_zoom_plus_stroke
    to start wireless networking.

  5. In the Device List view, select the BACnet/IP controllers to make the connection.

Using the eCommission application, you can now perform tasks on the connected BACnet/IP controllers as needed.

  • Connection Workflow for the eCommission Application
  • Cannot Connect Using Mobile Device with Data Plan