earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Explicación de procesos

Explicación de procesos


Productos WebStation
Funcionalidades: Dashboards
Versión del producto: 3.2, 3.3, 2022, 2023
14/03/2024

Cómo configurar y editar un periodo sobre el gráfico de periodo

Es posible configurar un periodo sobre el gráfico de periodo para comparar registros de tendencias en diferentes periodos de tiempo.

Mostrar más
action_close

Dashboard widgets are small applications in a dashboard. Dashboard widgets are the main components in a dashboard and present graphical information from your system.

You can create one or many dashboard widgets in a dashboard. Dashboard widgets can only be created in a dashboard in WebStation.

Ready to use

All dashboard widgets are ready to use. The only thing you must do is add the trend log, variable, alarm, or event you want to display in the dashboard widget. All dashboard widgets have default setting for color and different layout components, but you can also configure them to suit your needs. For example, you can add captions to the widget itself or the x- and y-axis in diagram, you can use different colors for different values or value ranges in a gauge.

Clone Widgets and Rebind Widget References

You can clone widgets and rebind widgets references.

Para obtener más información, consulte Clonar widgets y volver a vincular referencias de widget .

Empty Space

Empty space is not a dashboard widget but a way to create empty spaces between dashboard widgets. Empty spaces are used when you do the layout of a dashboard.

Alarm Count

An alarm count displays the number of alarms from the EcoStruxure Building Operation system.

Para obtener más información, consulte Recuento de alarmas .

Alarm Pareto Chart

An alarm Pareto chart is a graphical representation of alarms represented by bars but also by a cumulative line. An alarm pareto chart gives you a quick overview of the most common causes of alarms.

Para obtener más información, consulte Gráfica de Pareto de alarmas .

Alarm Pie

An alarm pie chart is a circular graphic divided into slices to illustrate proportions of alarms.

Para obtener más información, consulte Gráfico de alarmas .

Alarm Sankey Chart

An alarm Sankey chart is used to graphically present a Sankey chart of the alarms in the EcoStruxure Building Operation system.

Para obtener más información, consulte Gráfico de Sankey de alarmas .

Event Pareto Chart

An event Pareto chart is a graphical representation where the events are represented by bars but also by a cumulative line. An event pareto chart gives you a quick overview of the most common events.

Para obtener más información, consulte Gráfico de Pareto de eventos .

Event Pie

An event pie chart is a circular graphic divided into slices to illustrate proportions of events.

Para obtener más información, consulte Event Pie .

Event Rate Chart

An event rate chart is a graphical representation of event rates represented by bars.

Para obtener más información, consulte Gráfico de tasa de eventos .

Event Sankey Chart

An events Sankey chart is used to graphically present a Sankey chart of the events in the EcoStruxure Building Operation system.

Para obtener más información, consulte Gráfico de Sankey de eventos .

Heat Map

A heat map is a graphical representation of data where the values contained in a matrix are represented as colors.

Para obtener más información, consulte Mapa de calor .

Log Gauge

A log gauge displays trend log values in a gauge.

Para obtener más información, consulte Indicador de registro .

Log Pie

A log pie chart is a circular graphic divided into slices to illustrate proportions of trend logs.

Para obtener más información, consulte Gráfico circular de registro .

Log Value

A log value displays one or many trend log values as numerical values.

Para obtener más información, consulte Valor de registro .

Period Chart

A period chart is used to compare trend logs over different time periods.

Para obtener más información, consulte Gráfico de periodo .

Period over Period Chart

A period chart is used to compare trend logs over different time periods.

Para obtener más información, consulte Periodo sobre gráfico de periodo .

Point Gauge

A point gauge is used to graphically display a current value in a gauge.

Para obtener más información, consulte Indicador de punto .

Point Pie

A point pie chart is a circular graphic divided into slices to illustrate proportion of values.

Para obtener más información, consulte Gráfico circular de valores .

Point Value

A point value is used to display the present value of one or many variables as a numerical value.

Para obtener más información, consulte Valor de punto .

XY Plot

A XY plot, also called a scatter plot, is used to display values for two trend logs.

Para obtener más información, consulte Diagrama XY .

Browse

Use Browse to navigate to a graphic or a hyperlink that you want to add to a dashboard.

Dynamic Dashboad Widget

Dynamic widgets is a way to automatically add graphics to a dashboard using a search function.

Para obtener más información, consulte Widgets dinámicos .

Graphics

Graphics can be added to a dashboard.

Para obtener más información, consulte Gráficos en los paneles .

Hyperlinks

Hyperlinks can also be added to a dashboard. To be able to display the content of the hyperlink, you must enable external content to be embedded in WebStation.

Para obtener más información, consulte Configuring Security in WebStation using WorkStation .

Cómo configurar un periodo sobre un gráfico de periodo
  1. Haga clic en Configurar o haga clic en el botón Preferencias

     
    action_zoom_plus_stroke
    .

  2. Haga clic en Añadir .

  3. Seleccione los registros de tendencias y haga clic en Seleccionar .

  4. En el cuadro Tipo de gráfico , seleccione cómo se va a mostrar el registro de tendencias.

  5. En el cuadro Método de cálculo , seleccione un método de cálculo para el gráfico de tendencias.

  6. En el cuadro Color , introduzca un color para el registro de tendencias.

  7. Seleccione la posición del eje Y.

  8. En la lista Datos ausentes , seleccione cómo procesar los datos que faltan en el gráfico.

  9. En el cuadro Periodo , seleccione un periodo.

  10. En el cuadro Leyenda , escriba una leyenda.

  11. En el cuadro Enlace de imagen , introduzca un enlace a un objeto que sea relevante para el periodo sobre el gráfico de periodo.

  12. En el cuadro Mostrar leyenda , seleccione Verdadero para que se muestren el nombre y el color del registro de tendencias del periodo sobre el gráfico de periodo.

  13. En el cuadro Mostrar periodo , seleccione Verdadero para mostrar el periodo en forma de leyenda.

  14. En Apilar series , seleccione Verdadero para apilar las barras de series.

  15. En el cuadro Eje Y mínimo , introduzca el valor mínimo del eje Y izquierdo.

  16. En el cuadro Eje Y máximo , introduzca el valor máximo del eje Y izquierdo.

  17. En el cuadro Decimal , seleccione el número de decimales.

  18. Haga clic en Aceptar .

  • Cómo funcionan los paneles
  • Dashboard Widgets
  • Periodo sobre gráfico de periodo
  • Propiedades del período sobre gráfico de período - Cuadro de diálogo
  • Cómo añadir un widget a un panel